AKD-C Display Codes
During drive operation the drive display shows the following codes depending on the drive status. The AKD-C has one LED. All codes with more than one character are displayed sequentially.
|
Display Code |
Status |
|---|---|
|
No system power (inrush opened). |
|
Strings not fully powered (inrush closed). AKD-Ns cannot be enabled. The AKD-C has a fault which disables the AKD-Ns and unpowers the strings. |
|
Strings powered and drives disabled. AKD-Ns cannot be enabled. The AKD-C has a fault which only disables the AKD-N's control board temperature. |
|
Strings powered and drive operational. All AKD-Ns can be enabled. The AKD-C has no faults and strings are fully powered. |
+ [3 digit code, flashing] |
Fault (see Fault and Warning Messages). |
+ [3 digit code, flashing] |
Warning (see Fault and Warning Messages). |
|
|
Displaying drive IP address . |
|
|
Powered on and FPGA |
|
Drive enabled. |
|
Download code. |
|
|
Special mode: Burn-in. |
|
Kernel error. |
|
Resident loading. |
|
Resident completed and waiting for the operational to start. |
+ [3 digit code, flashing]
+ [3 digit code, flashing]
+ [IP address]